AXIS#.SAFE.SBT.ERROR

Description

Read the error of the Safe Brake Test (SBT) on the specified axis. The return value can be one of the following:

Value

Description

0

No error.

1

Fail to start the safe brake test. To start safe brake test, the axis must be enabled, the attached brakes must be released, and the axis must be at standstill.

2

Brakes are not released. To start safe brake test, the axis must be enabled, the attached brakes must be released, and the axis must be at standstill.

3

Fail to apply the brake. To find which brakes failed, see BRAKE#.SAFE.SBT.STATE.

4

Fail to release the brake. To find which brakes failed, see BRAKE#.SAFE.SBT.STATE.

5

Fail to apply current on the axis.

6

Motion limit exceed. Brake may be broken. To find which brakes failed, see BRAKE#.SAFE.SBT.STATE.

7

Current feedback out of range. To find which brakes failed, see BRAKE#.SAFE.SBT.STATE.

8

Communication error between the non-safe system part and the SMM.

9

Timeout. The safe brake test wasn’t able to complete.

10

System error on the SMM.

11

Interrupted by user.

12

Measured load is bigger than the configured maximum load.

255

Unknown error.

Code

--> AXIS1.SAFE.SBT.ERROR
0

Context

For complete SBT information refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

0 - 11
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
AXIS1.SAFE.SBT.ERROR

40f1h

01h

Unsigned8

-

-

Read only

No

AXIS2.SAFE.SBT.ERROR

40f1h

02h

Unsigned8

-

-

Read only

No